# MCUXpresso Task Definition An MCUXpresso task, or a list of tasks, must respect a JSON schema defined by the MCUXpresso for VS Code extension. Files that respect the following pattern `mcuxpresso-tasks*.json` are automatically validated against the schema, when opened and edited within VS Code. Also, all tasks added in `tasks.json` that are MCUXpresso-specific (i.e. `"type": "MCUXpresso"`) are also validated against the same schema. There are multiple actions that can be performed using the MCUXpresso task system, and each of the actions requires a specific set of command options to be defined. The command options are defined within the `commandOptions` property of the task object. ## MCUXpresso Task Each task needs at least the `"type"`, `"version"`, `"label"`, and `"commandOptions"` properties. The `"runOptions"` property is optional but it allows controlling the execution details of the task. The sections below list the available commands and their required options. ### High-level view of the basic properties | Property | Type | Required | Description | | -------- | ---- | -------- | ----------- | | type | "MCUXpresso" | ✓ | MCUXpresso task type. | | version | string | ✓ | MCUXpresso task version. | | label | string | ✓ | The task label. This will be displayed in the Terminal view inside VS Code. | | description | string | | Optional description of the MCUXpresso task's purpose and functionality. | | id | string | | Optional ID that can be assigned and help to uniquely identify the task within a sequence of tasks. | | runOptions | object | | Options that help controlling various aspects of the task execution. | |     awaitPreviousTasksCompletion | boolean | | Whether to wait for all the previous async tasks to complete before starting current task. By default, previous tasks are not awaited for completion. | |     awaitTaskCompletion | boolean | | Whether to wait for the task to complete before starting the next task. By default, task is awaited for completion. | |     executionDelay | number | | Delay execution of current task with the given number of seconds. By default, no delay is applied. | |     executionTimeout | number | | Timeout (in seconds) for current task execution. Task will be terminated once timeout occurs. A non-negative and non-zero value is valid. By default, no timeout is used. | |     retryCount | number | | If task fails, retry for the specified number of times. Retrying might help in certain setups, for example when retrieving data over an unreliable network connection. By default, no retries are performed. | |     skip | boolean | | Whether to skip the task. By default, task is executed. | |     taskOutputFile | string | | Path to a file that will contain the task's output. By default, a temporary file is automatically created. | | commandOptions | object (combined) | ✓ | See specific command details below | ### Available commands The `commandOptions` property defines the specific command to execute and its parameters. #### Base Command Property | Property | Type | Required | Description | | -------- | ---- | -------- | ----------- | | command | "installDependencies" | "installRemoteRepo" | "installRemoteStandalonePackage" | "installLocalRepo" | "installLocalArchive" | "installAchProduct" | "uninstallRepo" | "importExampleFromRepo" | "importProject" | "removeProject" | "buildProject" | "cleanProject" | "rebuildProject" | "eraseFlash" | "programFlash" | "runDebugProject" | ✓ | The MCUXpresso command to execute. | ### Description of individual commands The section below provides details about each of the command type supported by the MCUXpresso for VS Code extension. #### Command: `"installDependencies"` Properties supported by the "installDependencies" command: | Property | Type | Required | Description | | -------- | ---- | -------- | ----------- | |     command | "installDependencies" | ✓ | ID of the command. | |     dependencyType | "sdkDeveloper" | "zephyrDeveloper" | "matterDeveloper" | "debugSupport" | ✓ | Types of dependencies valid for "installDependencies" task. | #### Command: `"installRemoteRepo"` Properties supported by the "installRemoteRepo" command: | Property | Type | Required | Description | | -------- | ---- | -------- | ----------- | |     command | "installRemoteRepo" | ✓ | ID of the command. | |     repoDestinationPath | string | ✓ | Destination path used by "installRemoteRepo" task. | |     repoManifestFile | string | | Manifest file used by "installRemoteRepo" task. | |     repoRevision | string | ✓ | Repository revision used by "installRemoteRepo" task. | |     repoType | "mcuxsdk_2.x" | "mcuxsdk" | "mcuxsdk_int" | "zephyr" | "zephyr_nxp" | "matter" | "matter_nxp" | ✓ | Repository type used by "installRemoteRepo" task. | #### Command: `"installRemoteStandalonePackage"` Properties supported by the "installRemoteStandalonePackage" command: | Property | Type | Required | Description | | -------- | ---- | -------- | ----------- | |     command | "installRemoteStandalonePackage" | ✓ | ID of the command. | |     packageDestinationPath | string | ✓ | Installation package path used by "installRemoteStandalonePackage" task. | |     packageJsonFile | string | ✓ | JSON file name associated to the desired package used by "installRemoteStandalonePackage" task. See https://mcuxpresso.nxp.com/vscode/NXP.json for all the available packages. | |     packageVersion | string | ✓ | Version of the package installed via "installRemoteStandalonePackage" task. | #### Command: `"installLocalRepo"` Properties supported by the "installLocalRepo" command: | Property | Type | Required | Description | | -------- | ---- | -------- |----------- | |     command | "installLocalRepo" | ✓ | ID of the command. | |     repoPath | string | ✓ | Path to the local repository used by "installLocalRepo" task. | #### Command: `"installLocalArchive"` Properties supported by the "installLocalArchive" command: | Property | Type | Required | Description | | -------- | ---- | -------- | ----------- | |     command | "installLocalArchive" | ✓ | ID of the command. | |     archiveDestinationPath | string | ✓ | Archive installation path used by "installLocalArchive" task. | |     archivePath | string | ✓ | Archive path used by "installLocalArchive" task. | #### Command: `"installAchProduct"` | Property | Type | Required | Description | | -------- | ---- | -------- | ----------- | |     command | "installAchProduct" | ✓ | ID of the command. | |     destinationPath | string | ✓ | Product destination path used by "installAchProduct" task. | |     productID | string | ✓ | Remote ID of ACH product used by "installAchProduct" task. | |     productName | string | ✓ | Product name used by "installAchProduct" task. Will be appended to "destinationPath". | |     toolchainPath | string | | Toolchain path used by the "installAchProduct" task, required for non-Zephyr projects imported from ACH repository. | |     zephyrSdkPath | string | | Zephyr SDK path used by the "installAchProduct" task, required for Zephyr projects imported from ACH repository. | #### Command: `"uninstallRepo"` Properties supported by the "uninstallRepo" command: | Property | Type | Required | Description | | -------- | ---- | -------- | ----------- | |     command | "uninstallRepo" | ✓ | ID of the command. | |     deleteFromDisk | boolean | | Whether to delete repository from disk once task is executed. By default, repo is not deleted from disk. | |     repoPath | string | ✓ | Path to the repository to uninstall. | #### Command: `"importExampleFromRepo"` Properties supported by the "importExampleFromRepo" command: | Property | Type | Required | Description | | -------- | ---- | -------- | ----------- | |     command | "importExampleFromRepo" | ✓ | ID of the command. | |     appType | "inRepository" | "inWorkspace" | "freestanding" | "standalone" | ✓ | Application type to be created by the "importExampleFromRepo" task. See the official MCUXpresso for VS Code documentation to understand what type of projects can be created depending on the repository type. | |     boardID | string | ✓ | Board ID used by the "importExampleFromRepo" task. | |     exampleLocation | string | ✓ | Folder name for a workspace application, or the full path for freestanding and standalone applications. Used by the "importExampleFromRepo" task. | |     importedProjectName | string | ✓ | Project name of the example imported using the "importExampleFromRepo" task. | |     outOfTreeBoardsDir | string | | Custom board folder used by "importExampleFromRepo" task. | |     repoPath | string | ✓ | Path to the repository containing the example. | |     repoTemplateID | string | ✓ | ID of the template example imported using the "importExampleFromRepo" task. | |     toolchainPath | string | ✓ | Toolchain or Zephyr SDK path used by the "importExampleFromRepo" task. | #### Command: `"importProject"` Properties supported by the "importProject" command: | Property | Type | Required | Description | | -------- | ---- | -------- | ----------- | |     command | "importProject" | ✓ | ID of the command. | |     projectDestinationPath | string | ✓ | Project destination path used by "importProject" task. | |     projectPath | string | ✓ | Project path used by "importProject" task. | |     repoPath | string | | Repository path used by "importProject" task. | |     toolchainPath | string | | Toolchain or Zephyr SDK path used by "importProject" task. | #### Command: `"removeProject"` Properties supported by the "removeProject" command: | Property | Type | Required | Description | | -------- | ---- | -------- | ----------- | |     command | "removeProject" | ✓ | ID of the command. | |     deleteFromDisk | boolean | | Whether to delete project from disk once task is executed. By default, project is not deleted. | |     projectName | string | ✓ | Project name used by "removeProject" task. | #### Command: `"buildProject"` Properties supported by the "buildProject" command: | Property | Type | Required | Description | | -------- | ---- | -------- | ----------- | |     command | "buildProject" | ✓ | ID of the command. | |     buildConfigName | string | ✓ | Build configuration used by "buildProject" task. | |     buildConfigOverride | object | | Override settings used by "buildProject" task. | |         boardID | string | | Board ID. | |         buildDir | string | | Build directory. | |         cmakeExtraArgs | string | | Extra CMake arguments to be passed at build time. | |         debugConsole | "default" | "semihost" | "uart" | "none" | | Debug console type used by the application. | |     projectName | string | ✓ | Project name used by "buildProject" task. | #### Command: `"cleanProject"` Properties supported by the "cleanProject" command: | Property | Type | Required | Description | | -------- | ---- | -------- | ----------- | |     command | "cleanProject" | ✓ | ID of the command. | |     buildConfigName | string | ✓ | Build configuration used by "cleanProject" task. | |     buildConfigOverride | object | | Override settings used by "cleanProject" task. | |         boardID | string | | Board ID. | |         buildDir | string | | Build directory. | |         cmakeExtraArgs | string | | Extra CMake arguments to be passed at clean time. | |         debugConsole | "default" | "semihost" | "uart" | "none" | | Debug console type used by the application. | |     projectName | string | ✓ | Project name used by "cleanProject" task. | #### Command: `"rebuildProject"` Properties supported by the "rebuildProject" command: | Property | Type | Required | Description | | -------- | ---- | -------- | ----------- | |     command | "rebuildProject" | ✓ | ID of the command. | |     buildConfigName | string | ✓ | Build configuration used by "rebuildProject" task. | |     buildConfigOverride | object | | Override settings used by "rebuildProject" task. | |         boardID | string | | Board ID. | |         buildDir | string | | Build directory. | |         cmakeExtraArgs | string | | Extra CMake arguments to be passed at rebuild time. | |         debugConsole | "default" | "semihost" | "uart" | "none" | | Debug console type used by the application. | |     projectName | string | ✓ | Project name used by "rebuildProject" task. | #### Command: `"eraseFlash"` Properties supported by the "eraseFlash" command. | Property | Type | Required | Description | | -------- | ---- | -------- | ----------- | |     command | "eraseFlash" | ✓ | ID of the command. | |     debugConfigName | string | | Debug configuration name to be used by the "eraseFlash" task. | |     debugConfigOverride | object | | Override settings from debug configuration, used by the "eraseFlash" task. | |     probeSN | string | ✓ | Probe serial number to be used by the "eraseFlash" task. | |     projectName | string | ✓ | Project name used by "eraseFlash" task. | #### Command: `"programFlash"` Properties supported by the "programFlash" command. | Property | Type | Required | Description | | -------- | ---- | -------- | ----------- | |     command | "programFlash" | ✓ | ID of the command. | |     baseAddressHex | string | | Base address (hex format) for the file that will be programmed by the "programFlash" task. | |     debugConfigName | string | | Debug configuration name to be used by the "programFlash" task. | |     debugConfigOverride | object | | Override settings from debug configuration, used by the "programFlash" task. | |     eraseAllFlash | boolean | | Whether to erase all flash during execution of "programFlash" task. | |     fileToProgram | string | | Path to the binary/executable file to be programmed by the "programFlash" task. | |     probeSN | string | ✓ | Probe serial number to be used by the "programFlash" task. | |     projectName | string | ✓ | Project name used by "programFlash" task. | |     resetTargetOnExecution | boolean | | Whether to reset target after the completion of the "programFlash" task. | #### Command: `"runDebugProject"` Properties supported by the "runDebugProject" command: | Property | Type | Required | Description | | -------- | ---- | -------- | ----------- | |     command | "runDebugProject" | ✓ | ID of the command. | |     appOutputFile | string | | Application output file path to be used by the "runDebugProject" task. By default, a temporary file is created. | |     debugConfigName | string | | Debug configuration name to be used by the "runDebugProject" task. | |     debugConfigOverride | object | | Override settings from debug configuration, used by the "runDebugProject" task. | |     probeSN | string | ✓ | Probe serial number to be used by the "runDebugProject" task. | |     projectName | string | ✓ | Project name used by "runDebugProject" task. | |     terminatePattern | string | | Terminate pattern used by the "runDebugProject" task. | |     terminateTimeout | number | | Terminate timeout used by the "runDebugProject" task. By default, 60 seconds is the default timeout. |