# MCUXpresso Installer In addition to the extension itself, some extra tools and software components are required for the full development flow within VS Code. All of these dependencies are managed by the MCUXpresso Installer tool, designed to guide you through the installation process. When clicking *Open MCUXpresso Installer* from QUICKSTART PANEL view, if the extension does not find it, it automatically downloads and starts the tool. Alternatively, you can download MCUXpresso Installer tool from the following links: - [Windows](https://www.nxp.com/lgfiles/updates/mcuxpresso/MCUXpressoInstaller.exe) - [Ubuntu](https://www.nxp.com/lgfiles/updates/mcuxpresso/MCUXpressoInstaller.deb.bin) - [macOS_x64](https://www.nxp.com/lgfiles/updates/mcuxpresso/MCUXpressoInstaller.dmg) - [macOS_arm64](https://www.nxp.com/lgfiles/updates/mcuxpresso/MCUXpressoInstaller_arm64.dmg) After installation, the Installer layout can be found in the following locations: - Windows: **%userprofile%\AppData\Local\Programs\MCUXpressoInstaller** - Linux: **$HOME/MCUXpressoInstaller** - macOS: The Installer is **a disk image file** (.dmg) and can be easily mounted in **/Applications** by dragging and dropping the Installer icon >**Note:** On Linux systems, the Installer requires admin rights to configure the necessary permissions for the application. This provides options to install: - [Python](https://www.python.org)/[west](https://docs.zephyrproject.org/latest/develop/west/index.html) to run scripts and understand complex repositories; - [git](https://git-scm.com) for the ability to clone source repositories and add version control; - [ninja](https://ninja-build.org), [cmake](https://cmake.org) for build process infrastructure; - [Zephyr SDK](https://docs.zephyrproject.org/latest/develop/toolchains/zephyr_sdk.html) minimal bundle if you want to develop applications based on Zephyr. Also, some additional [libraries and tools](https://docs.zephyrproject.org/latest/develop/getting_started/index.html) are required for build process; - [GNU Arm Toolchain](https://developer.arm.com/Tools%20and%20Software/GNU%20Toolchain) if you want to develop applications based on [MCUXpresso SDK](https://www.nxp.com/design/software/development-software/mcuxpresso-software-and-tools-/mcuxpresso-software-development-kit-sdk:MCUXpresso-SDK); on top of the toolchain, additional NXP libraries and headers are provided to facilitate various extra features like semihosting stubs, macros to create MTB support (for Cortex M0+), macros to allow code/data to be placed into alternate memory banks, etc; - [LinkServer](https://www.nxp.com/design/software/development-software/mcuxpresso-software-and-tools-/linkserver-for-microcontrollers:LINKERSERVER), [Segger J-Link](https://www.segger.com/) and [PEmicro](https://www.pemicro.com) debug probes software support; - [MCUXpresso Configuration Tools](https://www.nxp.com/design/design-center/software/development-software/mcuxpresso-software-and-tools-/mcuxpresso-config-tools-pins-clocks-and-peripherals:MCUXpresso-Config-Tools) to allow developers to quickly build a custom SDK and leverage pins, clocks and peripherals to generate initialization C code or register values for custom board support. - [MCUXpresso SEC Secure Provisioning Tool](https://www.nxp.com/design/design-center/software/development-software/mcuxpresso-software-and-tools-/mcuxpresso-secure-provisioning-tool:MCUXPRESSO-SECURE-PROVISIONING) to simplify generation and provisioning of bootable executables on NXP MCU devices. - [GUI Guider](https://www.nxp.com/design/design-center/software/development-software/gui-guider:GUI-GUIDER) HMI design tool for embedded GUI and host-side FreeMASTER visualization design using LVGL. - [FreeMASTER](https://www.nxp.com/design/design-center/software/development-software/freemaster-run-time-debugging-tool:FREEMASTER) tool for real-time debug monitor that enables runtime visualization and control of application variables. MCUXpresso Installer involves a few steps, aiming to install (or upgrade to a minimal required version) the dependencies. ## Default view ![MCUXpresso Installer](./pictures/nxp-installer.png) You can select one or multiple items from the available list. Once at least one package is selected, the two top-right buttons "Install" and "Show details" become enabled. In order to select the version of the package to be installed, you can click on the dropdown menu next to each package. This allows you to choose between different available versions. ![MCUXpresso Installer](./pictures/nxp-installer-version-select.png) The "Install" button installs all components from selected packages that do not already exist at the required versions. ## Custom view ![MCUXpresso Installer](./pictures/nxp-installer-details.png) Clicking the "Show details" button opens a panel on the right side, displaying all components from the selected packages. The component list is interactive. Individual components can be added or removed to customize the toolset to be installed. Selection can include one, multiple, or all components across one or more packages. The "Install" button operates on the customized list of components, not on the full package bundles. When one or more components are selected or deselected, the corresponding parent package is marked as partially selected (indeterminate state). When all components within a package are selected or deselected, the parent package is automatically marked as selected or deselected, respectively. Similarly, when a package is selected or deselected, all of its components are selected or deselected accordingly. Component dependencies across packages are managed automatically. Some components (e.g. Git, Python) appears in multiple packages (e.g. Zephyr Developer, MCUXpresso SDK Developer). Their selection states are synchronized — selecting or deselecting one, mirrors the change in the others. If a full package is selected, its components are also selected in other packages where they are present. Special case: to avoid inconsistencies, when a package is deselected, its components are deselected only within that package - they remain unchanged in other packages. The detailed panel is shown when the user clicks "Show details", and hidden when the "Hide details" button is clicked. ## Software kits environments - **MCUXpresso SDK Developer** - it contains necessary dependencies for users targeting to develop applications based on [MCUXpresso SDK](https://mcuxpresso.nxp.com). - **Zephyr Developer** - aims to create an environment for [Zephyr RTOS](https://www.zephyrproject.org/) based applications. - **Matter Developer** - includes the necessary components that must be installed to set up a development environment for [Matter](https://project-chip.github.io/connectedhomeip-doc/index.html) applications. ### MCUXpresso Virtual Environment Pip, west and other Python requirements are installed in a Python virtual environment located on: - Windows: %userprofile%/.mcuxpressotools - Linux and macOS: $HOME/.mcuxpressotools The Python virtual environment name includes the Python version used to create the virtual environment. (for example: .venv_3_10) The steps performed by the Installer with an installed Python 3.10 to create a development environment for Zephyr can be manually run: Windows: 1. Open a cmd.exe terminal window 2. Create a virtual environment: ```console python -m venv %userprofile%/.mcuxpressotools/.venv_3_10 ``` 3. Activate the virtual environment: ```console %userprofile%/.mcuxpressotools/.venv_3_10/Scripts/activate.bat ``` 4. Install pip ```console python -m ensurepip --upgrade ``` 5. Install west: ```console pip install west --upgrade ``` 6. Zephyr’s requirements files declare additional Python dependencies. Download and install the requirements using pip. ```console wget https://github.com/zephyrproject-rtos/zephyr/tree//scripts/requirements.txt wget https://github.com/zephyrproject-rtos/zephyr/tree//scripts/requirements-base.txt wget https://github.com/zephyrproject-rtos/zephyr/tree//scripts/requirements-build-test.txt wget https://github.com/zephyrproject-rtos/zephyr/tree//scripts/requirements-compliance.txt wget https://github.com/zephyrproject-rtos/zephyr/tree//scripts/requirements-extras.txt wget https://github.com/zephyrproject-rtos/zephyr/tree//scripts/requirements-run-test.txt pip install -r ./requirements.txt ``` Linux: 1. Use apt to install Python venv package: ```console sudo apt install python3-venv ``` 2. Create a virtual environment: ```console python3 -m venv $HOME/.mcuxpressotools/.venv_3_10 ``` 3. Activate the virtual environment: ```console source $HOME/mcuxpressotools/.venv/bin/activate ``` 4. Install pip ```console python -m ensurepip --upgrade ``` 5. Install west: ```console pip install west --upgrade ``` 6. Zephyr’s requirements files declare additional Python dependencies. Download and install the requirements using pip. ```console wget https://github.com/zephyrproject-rtos/zephyr/tree//scripts/requirements.txt wget https://github.com/zephyrproject-rtos/zephyr/tree//scripts/requirements-base.txt wget https://github.com/zephyrproject-rtos/zephyr/tree//scripts/requirements-build-test.txt wget https://github.com/zephyrproject-rtos/zephyr/tree//scripts/requirements-compliance.txt wget https://github.com/zephyrproject-rtos/zephyr/tree//scripts/requirements-extras.txt wget https://github.com/zephyrproject-rtos/zephyr/tree//scripts/requirements-run-test.txt pip install -r ./requirements.txt ``` macOS: 1. Create a virtual environment: ```console python3 -m venv $HOME/.mcuxpressotools/.venv_3_10 ``` 2. Activate the virtual environment: ```console source $HOME/.mcuxpressotools/.venv_3_10/bin/activate ``` 3. Install pip ```console python -m ensurepip --upgrade ``` 4. Install west: ```console pip install west --upgrade ``` 5. Zephyr’s requirements files declare additional Python dependencies. Download and install the requirements using pip. ```console wget https://github.com/zephyrproject-rtos/zephyr/tree//scripts/requirements.txt wget https://github.com/zephyrproject-rtos/zephyr/tree//scripts/requirements-base.txt wget https://github.com/zephyrproject-rtos/zephyr/tree//scripts/requirements-build-test.txt wget https://github.com/zephyrproject-rtos/zephyr/tree//scripts/requirements-compliance.txt wget https://github.com/zephyrproject-rtos/zephyr/tree//scripts/requirements-extras.txt wget https://github.com/zephyrproject-rtos/zephyr/tree//scripts/requirements-run-test.txt pip install -r ./requirements.txt ``` ### MCUXpresso Venv Terminal Shortcut The desktop shortcut feature automatically creates shortcuts on the user's desktop when MCUXpresso Installer is installed on the user system. ![MCUXpresso Installer](./pictures/nxp-installer-venv-shortcut.png) These shortcuts provide direct access to activate and use the virtual environments without navigating through complex file structures. Also, the shortcut provides the option to choose between multiple virtual environments. ![MCUXpresso Installer](./pictures/nxp-installer-venv-terminal.png) The feature is available on all platforms: - Windows: A desktop shortcut on the Windows desktop - Linux: A desktop shortcut in the user's desktop environment - macOS: An application included in the disk image file ## ARM components - [**Arm GNU Toolchain**](https://developer.arm.com/Tools%20and%20Software/GNU%20Toolchain) - toolchain for MCUXpresso SDK development plus NXP extension pack used to provide extra functionalities (i.e. additional runtime libraries, semihosting, trace, multicore, etc.). - **Standalone Toolchain Add-ons** - NXP toolchain extension pack used to provide extra functionalities that can be used on top of an Arm GNU Toolchain distribution (i.e. runtime libraries, semihosting, trace, multicore, etc.). Although it is built and tested with a particular baseline version of Arm GNU Toolchain (which also gives this pack version number) it can be also copied on top of a user custom Arm GNU Toolchain version in order to benefit on all provided MCUXpresso for VS Code extension functionalities. To achieve this, be sure the content of this archive is unzipped and copied on top of the desired Arm GNU Toolchain root installed file layout. >**Note:** Multiple versions of [**Arm GNU Toolchain**](https://developer.arm.com/Tools%20and%20Software/GNU%20Toolchain) and **Standalone Toolchain Add-ons** are available to download and install.\ The latest version of the **ARM Components** is available on all operating systems, while version 13.2 is unavailable on **Ubuntu 24.04** due to missing system dependencies. ## Debug probes software - [**LinkServer**](https://www.nxp.com/design/software/development-software/mcuxpresso-software-and-tools-/linkserver-for-microcontrollers:LINKERSERVER) - GDB server and low level debug utilities for NXP debug probes. - [**Segger J-Link**](https://www.segger.com/) - software pack for J-Link debug probes. - [**PEmicro**](https://www.pemicro.com) - PEmicro's GDB Server to debug supported NXP ARM Cortex-M processor targets ## Standalone Tools - [**MCUXpresso Configuration Tools**](https://www.nxp.com/design/design-center/software/development-software/mcuxpresso-software-and-tools-/mcuxpresso-config-tools-pins-clocks-and-peripherals:MCUXpresso-Config-Tools) - pin, clock, peripheral, memory and trusted execution configuration utilities. - [**MCUXpresso Secure Provisioning Tool**](https://www.nxp.com/design/design-center/software/development-software/mcuxpresso-software-and-tools-/mcuxpresso-secure-provisioning-tool:MCUXPRESSO-SECURE-PROVISIONING) - GUI and utilities for securing application code and provisioning devices. - [**GUI Guider**](https://www.nxp.com/design/design-center/software/development-software/gui-guider:GUI-GUIDER) - HMI design tool for embedded GUI and host-side FreeMASTER visualization design using LVGL. - [**FreeMASTER**](https://www.nxp.com/design/design-center/software/development-software/freemaster-run-time-debugging-tool:FREEMASTER) - Real-time debug monitor that enables runtime visualization and control of application variables. ## Package and component status, version and updates Each package and component indicates with a colored badge its update status as following: - ![greenbadge](./pictures/nxp-installer-badge-green.png) **(green badge)**: package or component is up to date. Tooltip indicates the installed version of component or, in case of package, the installed version for each component. ![MCUXpresso Installer Component Updated](./pictures/nxp-installer-comp-updated.png) - ![graybadge](./pictures/nxp-installer-badge-gray.png) **(gray badge)**: package or component missing. Tooltip indicates each component, its status and installed version. If this component or package is needed, select it and install it. ![MCUXpresso Installer Component Missing](./pictures/nxp-installer-comp-missing.png) - ![yellowbadge](./pictures/nxp-installer-badge-yellow.png) **(yellow badge)**: package or component with an older version than the latest one available. Tooltip indicates component installed version and newer available version. If this component is intended to be used, it is recommended to update it. In case of package, the tooltip indicates which components have available updates. ![MCUXpresso Installer Component Lower](./pictures/nxp-installer-comp-lower.png) - ![bluebadge](./pictures/nxp-installer-badge-blue.png) **(blue badge)**: package or component with an older version than the latest one available. Tooltip indicates that the component needs a manual update. If this component is intended to be used, it is recommended to update it. In case of package, the tooltip indicates which components have available updates. ![MCUXpresso Installer Component Lower](./pictures/nxp-installer-comp-manual-update.png) - ![redbadge](./pictures/nxp-installer-badge-red.png) **(red badge)**: package or component does not meet minimum required version or the versions are incompatible. Tooltip indicates the minimum required version. If this component is intended to be used, it is highly recommended to update it. In case of package, the tooltip indicates which components need to be updated. ![MCUXpresso Installer Component Outdated](./pictures/nxp-installer-comp-outdated.png) Once the installation process starts, a console with a progress bar displays the status and execution details. The colored badge status is also updated at the end of installation process. ![MCUXpresso Installer Console](./pictures/nxp-installer-console.png) The console output displays details of where a tool is downloaded from and also the command used to install it. ![MCUXpresso Installer Console Details](./pictures/nxp-installer-console-details.png) If the Installer has updated the environment variables, then a pop-up alerts the user that a VS Code extension restart is needed to reflect the updated environment variables. ![MCUXpresso Installer Warning Env Variables](./pictures/nxp-installer-warn-env-variables.png) In case of errors, the console reports the encountered issues. If the cause of error can be fixed by user, pressing again the "Install" button restarts the previous component selection. The installer skips previously installed components after finding the minimal version exists. A check for component updates is available on toolbar, forcing a rescan of installed tools. ![MCUXpresso Installer Version Check](./pictures/nxp-installer-comp-check-updates.png) A context menu is available within the console area, to allow Select All / Copy and Clear operations over the generated log.\ All operations are also available as keyboard shortcuts:
  • Select All - Ctrl + A
  • Copy - Ctrl + C
  • Clear - Ctrl + X
![MCUXpresso Installer Console Menu](./pictures/nxp-installer-console-menu.png) ## Undoing the latest installation The **Undo latest installation** feature offers the possibility to automatically revert the components installed during the latest installation process. >**Revert** : Completely uninstall the specified component, maintaining the older versions of the component, which already existed prior to the latest installation process.\ The components able to maintain the older version are the ones installed under the `%USERPROFILE%(or $HOME on Unix systems)/.mcuxpressotools` location (such as *ARM GNU Toolchain*, *CMake*), or standalone tools which have individual installation locations for each version (such as *LinkServer*, *MCUXpresso Config Tools*).\ Global components or components which have a single location which is overwritten upon version update (such as *Git*, *7-Zip*, *PEMicro*) cannot maintain the previously installed version upon uninstall.\
The **PATH** environment variable is also returned to its value prior to the latest installation process, if applicable. The action can be triggered via the **Undo latest installation** button, located under the MCUXpresso Installer's **drop-down menu**.\ Upon successfully completing a component installation, the button becomes active. ![MCUXpresso Installer Undo Button](./pictures/nxp-installer-undo-button.png) Upon clicking the button, the user is prompted with the list of components which were successfully installed during the latest installation process. ![MCUXpresso Installer Undo Menu](./pictures/nxp-installer-undo-menu.png) Upon pressing **Continue**, the undo process begins for the specified components. >**Note:** Some components (such as *Git*, *7-Zip*, *Python*, *pip*, *west*, *Python dependencies*) currently present in the installation list are not influenced by the undo operation, as automatically tempering with these components can damage the **global** environment.\ After the completion of the undo process, a list of such components is presented to the user in the form of a **warning pop-up message**.\ These components can be **manually removed** by the user.\ ![MCUXpresso Installer Undo Warning](./pictures/nxp-installer-undo-warning.png) ## Dark/light theme From the top toolbar, user can switch between dark and light themes. ![MCUXpresso Installer Theme Dark](./pictures/nxp-installer-theme.png) ![MCUXpresso Installer Theme Light](./pictures/nxp-installer-theme-light.png)