# MCUXpresso Installer Troubleshooting The **MCUXpresso Installer Troubleshooting** guide is designed to help users quickly identify and resolve common issues encountered during the installation of development software tools dependencies. ## Table of Contents - [Python Installation](#python-installation) - [Python Virtual Environment](#python-virtual-environment) - [Python-Tk Library](#python-tk-library) - [Wget Utility](#wget-utility) - [Windows Developer Mode](#windows-developer-mode) ## Python Installation The installation process for Python can fail unexpectedly due to various reasons, usually related to system configuration. ### Common causes - Manual deletion of Python folders before uninstalling - Corrupted or incomplete Python installation - Conflicts with Windows App Execution Aliases - Missing registry entries or broken uninstall paths ### Recommended solutions #### 1. Use the Python Installer **Steps:** - Download the installer for the same Python version. - Run the installer and choose **Repair**. - After repair completes, run the installer again and choose **Uninstall**. #### 2. Use the Installed Apps Settings **Steps:** - Open **Settings → Apps → Installed Apps**. - Locate Python, click the three-dot menu → **Modify**. - Choose **Repair**, then repeat and choose **Uninstall**. #### 3. Disable App Execution Aliases **Steps:** - Open **Start → Manage App Execution Aliases**. - Disable all Python-related entries (e.g., `python.exe`, `python3.exe`). - Retry installation or uninstallation. #### 4. Clean Up Environment Variables **Steps:** - Open **System Properties → Environment Variables**. - Remove any `PYTHONPATH` or Python-related entries from both **User** and **System** variables. - Delete folders like: - `%USERPROFILE%\AppData\Local\Programs\Python\` - `%USERPROFILE%\AppData\Local\Programs\Python\PythonXX\Scripts\` ## Python Virtual Environment Issues can be encountered during the creation, updating, activation, or usage of the Python virtual environment. ### Common causes - Corrupted Python installation - Corrupted virtual environment - The already existing virtual environment is tied to a missing Python installation ### Recommended solutions #### 1. If the virtual environment does not already exist - Make sure that the correct version of **Python** is installed and functional by following the [Python Installation](#python-installation) troubleshooting guide. - Retry the creation of the virtual environment using the **MCUXpresso Installer**: - Open **MCUXpresso Installer**. - Perform a **check for newer versions of components**. - Install the **Python dependencies** for the desired package. #### 2. If the virtual environment already exists - Remove the existing virtual environment from `%USERPROFILE%(or $HOME on Unix systems)/.mcuxpressotools/.venv`. - Make sure that the correct version of **Python** is installed and functional by following the [Python Installation](#python-installation) troubleshooting guide. - Retry the creation of the virtual environment using the **MCUXpresso Installer**. - Open **MCUXpresso Installer**. - Perform a **check for newer versions of components**. - Install the **Python dependencies** for the desired package. ## Python-Tk Library Issues regarding the **python-tk** (python3-tk) library can occur on systems where **Python** is installed via the system's **package manager** - APT (Ubuntu) or Homebrew (macOS). ### Common causes - The **Python** installations from the system's **package manager** do not include the **python-tk** library. ### Recommended solutions #### 1. For APT-based systems (Ubuntu) - Open a **terminal** window - Install the **python3-tk** library:\ `sudo apt update`\ `sudo apt install python3-tk` - Verify the installation:\ `python3 -m tkinter` #### 2. For Homebrew-based systems (macOS) - Open a **terminal** window - Install the **python-tk** library for your installed **Python version** (e.g. 3.10, 3.13):\ `brew install python-tk@` - Verify the installation:\ `python3 -m tkinter` ## Wget Utility Issues regarding the installation of **Wget** can occur on systems where network connectivity is restricted or proxy configurations are modified. ### Common causes - Incomplete or misconfigured network settings - Proxy server restrictions - Firewall blocking download connections - Invalid or outdated SSL/TLS certificates ### Recommended solution #### Manual Wget download and configuration - Download Wget from an official mirror site - Add **Wget** to the **PATH** environment variable - Verify the installation by running `wget --version` in a new instance of the command prompt or terminal - Restart the **MCUXpresso Installer** application to ensure the new configuration takes effect ## Windows Developer Mode Some development tools require Windows Developer Mode to be enabled for proper functionality, particularly for debugging and development features. ### Recommended solutions #### 1. Enable Developer Mode through Settings **Steps:** - Open **Settings** (Windows key + I) - Navigate to **System → For developers** (Windows 11) or **Update & Security → For developers** (Windows 10) - Select **Developer mode** - Click **Yes** when prompted to confirm the change - Restart your computer if prompted #### 2. Enable Developer Mode through Registry (if Settings method fails) **Steps:** - Press **Windows key + R** and type `regedit` - Navigate to `HKEY_LOCAL_MACHINE\SOFTWARE\Microsoft\Windows\CurrentVersion\AppModelUnlock` - Create a new **DWORD (32-bit) Value** named `AllowDevelopmentWithoutDevLicense` - Set the value to **1** - Restart your computer #### 3. Verify Developer Mode is enabled **Steps:** - Open **Command Prompt** as Administrator - Run the command: `reg query "HKEY_LOCAL_MACHINE\SOFTWARE\Microsoft\Windows\CurrentVersion\AppModelUnlock" /v AllowDevelopmentWithoutDevLicense` - Verify the value is set to **0x1**