# Create Project PROJECTS view provides a suite of possibilities for creating or importing an application. Also, this view is responsible to manage the created projects in order to add/remove components, build, debug, remove existing ones. ## Import a project from source repository Once a [source repository](Import-Repository) is available in MCUXpresso for VS Code, you can create your own application by importing an example from the repository. You have several options to open the wizard to create a project: 1. Select the desired available repository within IMPORTED REPOSITORIES view, right-click on it and select "Import Example Application from an Installed Repository" or 2. From PROJECTS view (in case it has no projects yet) press "Import Example from Repository" button or 3. From PROJECTS view toolbar select "Import Example Application from an Imported Repository" option. ![Import Example](./pictures/nxp-import-example-application.png) Selecting one of the above options will open a wizard with few steps to follow until the project can be generated. ![Import Example Wizard](./animation/nxp-create-project.gif) You then have to fulfill some required fields: - **Choose a repository** - select from the imported source repository (can be MCUXpresso, Zephyr or a custom one) - **Choose a board** - select one listed here (the ones available within the selected repository) - **Choose a template** - this is the list of available project templates for selected repository/board from above - **App type** - application type selection - **Name** - project name. This will be further referred in the workspace. If the project's name already exists, an error will indicate this - **Location** - path for the project. The path will be created if not exists. This field is available, unless the application is kept in repository. - **Choose a toolchain** - select one of the already installed toolchains - **Open readme file after project is imported** - this option will open existing example readme in case it exists (when the project will be created, after pressing "Import" button); this option is unchecked by default ## Application Types The following application types are available depending on the selected repository type: - `Repository application` - application is located directly in the repository folder (example's source code will not be copied) - `Freestanding application` - example's source code will be copied in the destination folder - `Workspace application` - project is in the repository workspace (see [Zephyr Application Development](https://docs.zephyrproject.org/latest/develop/application/index.html) for details). - `Standalone application` - project is self-contained and independent of the repository.
 Repository Type   Application Type 
 Repository   Freestanding   Workspace   Standalone 
MCUXpresso SDK 2.x
MCUXpresso SDK 24.12 to 25.09
MCUXpresso SDK 25.12 and newer
Zephyr
Matter

If the "Application Type" field is not available, it means there is only a single option and this is chosen by default. >**Note:** For now, support for "Standalone application" is marked as "Experimental" and needs to be enabled first. To enable it go to Settings->Extensions->MCUXpresso for VS Code and check the "Enable Standalone Projects" checkbox. (import-an-existing-project)= ## Import an existing project Import an existing MCUXpresso project by selecting one of the following options: 1. From PROJECTS view (in case it has no projects yet) press "Import MCUXpresso for VS Code Project" button or 2. From PROJECTS view toolbar select "Import MCUXpresso for VS Code Project" option. ![Import Project](./pictures/nxp-import-project.png) From the wizard, select the existing project (choose from archived, folder project options or executable; choosing an executable file will result in creating a new project that will allow debugging and accessing the available binary tools options for that executable). ![Import Project Wizard](./pictures/nxp-import-project-wizard.png) You have to fill the required fields: - **Import path** - select the project archive path - **Destination** - select the path where the project will be imported - **Choose a repository** - select one of the already imported repositories which are compatible with the imported project type. Pick a suitable one or use *Add repository path* option from the combobox - **Choose a toolchain** - select one of the already installed toolchains. Pick a suitable one or use *Add toolchain path* option from the combobox ## Import a project based on an existing executable file To import a project from an existing executable press the "Executable" button from the import project wizard, choose the executable file and fill in the required information ( destination, toolchain). ![Import Executable Project](./pictures/nxp-import-executable-project.png) Since the newly created project won't contain any source files this project won't have the option to build/rebuild the project or to create any build configuration. However, the project can be debugged once a device target is associated with the project. This can be done by either associating a repository with the project or by simply starting a debug session and providing the necessary information. For example, on LinkServer the extension will first present a list of all the supported devices. ![LinkServer devices](./pictures/nxp-linkserver-devices.png) A project resulted from importing an executable file has the existing binary tools support: Image Info options and the tools from "Binary utilities" menu are available. ## Import an existing project from folder To import an existing project from folder choose "Folder" button from the import project wizard. ![Import Project from Folder](./pictures/nxp-import-project-folder.png) If the selected folder is an actual project, the path will be automatically filled in "Import Path" field. Otherwise, a quick pick will appear listing the available projects in the given folder plus its nested directories, recursively. User can choose only one project from the list, and the "Import Path" field will be filled accordingly. ![Import Project Quick Pick](./pictures/nxp-import-quick-pick.png) > **Note:** Importing projects from installed repositories is not available using "Import Project from Folder". To import an SDK project, please use the "Import Example from Repository" option. (export-a-project)= ## Export a project An existing project can be exported to an archive. This can be achieved by selecting a project, open context menu and select Project -> Export MCUXpresso Project Archive. ![Export Project Archive](./pictures/nxp-export-project.png) You'll be asked then to provide a path where the archive will be generated. The default is the path where the project is located. ## Move a project from one machine to another A project can be moved from one machine to another by using the export and import project features. First you need to export the desired project using [Export MCUXpresso Project Archive](#export-a-project) option. After that, you need to copy the generated project archive to the other machine. Once the project archive is available on the second machine, you can use the [Import Project Wizard](#import-an-existing-project) feature to import the project. After importing the project, the repository and toolchain paths are updated according to the values selected in the Import Project Wizard. The extension reports all paths in project settings files (files in `.vscode` project directory) that could not be automatically resolved. In this case, the user needs to manually update them. ![Invalid Paths](./pictures/nxp-import-project-invalid-paths.png) ## Build configuration The PROJECTS view displays all available build configurations for each project. One is selected by default, any other can be selected using "Set as Default" option. ![Build configurations](./pictures/nxp-build-configurations.png) Additionally, you can add, duplicate, edit or delete a build configuration. ![Build configurations options](./pictures/nxp-build-configuration-operations.png) ## Build project The next step is to build the executable file. Use **Build Selected** option from toolbar or right click on the desired project and select **Build selected**. This will start building the selected build configuration. The output generated files can be found in the VS Code Explorer view. ![Build option](./pictures/nxp-build.png) ## Debug configurations The PROJECTS view allows you to manage debug configurations for your projects. You can add, remove, duplicate, and edit debug launch configurations. Moreover, using the inline buttons associated to each debug configuration, you can easily start a debug session using the selected configuration. There is also a **Default** debug configuration that you can manually set. The default debug configuration will be used when you start a debug session by clicking the **Debug** button associated to the project. ![Debug configurations](./pictures/nxp-debug-configurations.png) When there is no **Default** debug configuration and the **Debug** button associated to a project is clicked, the extension will prompt you to select a debug configuration from a list of available configurations, if this is the case. The debug configuration selected using the quick-pick will be set as the default debug configuration for the project. ![Debug configuration selection](./pictures/nxp-debug-configuration-selection.png) Debug configuration editing is achieved by using the built-in VS Code editor. The MCUXpresso for VS Code extension will open `launch.json` file in a dedicated editor, and highlight the name of the specific debug configuration. ![Debug configuration editing](./pictures/nxp-debug-configuration-editing.png) ## Toolchain Management One important aspect is the toolchain management. This extension is able to identify existing MCUXpresso SDK or Zephyr installed toolchains, depending on the selected repository type, and can also detect the user-added options. Users can choose their preferred toolchain either during project creation or when configuring an existing project. ![Toolchain selection](./pictures/nxp-import-toolchain.png) Once the project is created, the toolchain selection is preserved in project settings, in JSON format in the file `mcux_include.json`. This file contains all variables for the `CMakePresets.json` file. ![Toolchain settings](./pictures/nxp-import-toolchain-settings.png) ### Changing the associated toolchain or Zephyr SDK for an existing project The associated toolchain or Zephyr SDK can be modified for an existing project. To change it, right-click on the project, navigate to "Configure", and select "Associate Toolchain" or "Associate Zephyr SDK". ![Associate toolchain](./pictures/nxp-associate-toolchain.png) ![Zephyr Associate SDK](./pictures/nxp-zephyr-associate-sdk.png) A quick pick menu will appear with the following options: 1. **Available toolchains or Zephyr SDKs** - Lists all toolchains or Zephyr SDKs currently installed on your system. 2. **Add toolchain path...** - Allows you to manually specify a custom toolchain location. 3. **Use recommended version** - Automatically detects and installs the recommended toolchain version for your project. This option ensures compatibility with the associated repository requirements. When selected, the extension will: - Detect the recommended toolchain version from the repository information. - Verify if the version is already installed on your system. - Initiate an automatic installation process if the version is not found. >**Note:** Automatic installation requires installer integration support to be enabled. See [Installer Integration NXP GitHub Documentation](./MCUXpresso-Installer-Integration.md) for more details. - Once the recommended version is installed and detected, it will be automatically associated with your project. 4. **Default Zephyr SDK** - Available only for Zephyr projects, this option allows you to use the default Zephyr SDK configuration, the build system will decide which Zephyr SDK to use from the installed ones. ![Associate toolchain options](./pictures/nxp-associate-toolchain-options.png) ![Zephyr SDK options](./pictures/nxp-zephyr-associate-sdk-options.png) ### Toolchain and Zephyr SDK version validation when building a project When building a project, if the associated toolchain or Zephyr SDK version does not match the recommended version for that project, the extension will display a warning notification. This ensures that your project builds with the correct toolchain or Zephyr SDK configuration and helps avoid potential compatibility issues. ![Toolchain version mismatch warning](./pictures/nxp-toolchain-version-warning.png) ![Zephyr SDK version mismatch warning](./pictures/nxp-zephyr-sdk-version-warning.png) The notification will show: - The current toolchain or Zephyr SDK version associated with your project. - The recommended toolchain or Zephyr SDK version for your project. - Options to update or keep the current version. Selecting "Yes" triggers an automatic update to the recommended version. The extension will detect and install the recommended version if needed, following the same workflow as the "Use recommended version" option detailed in the "Changing the associated toolchain or Zephyr SDK for an existing project" section above. ![Toolchain install notification](./pictures/nxp-toolchain-install-info.png) ![Zephyr SDK install notification](./pictures/nxp-zephyr-sdk-install-info.png) Selecting "No" maintains the currently associated version for your project. Additionally, you can select "Don't show again" to disable future version mismatch warnings for this specific project. ## Rename project You can rename a project in MCUXpresso for VS Code by right-clicking the project and selecting 'Project -> Rename Project' from the context menu and updating the project name in the quick input dialog. ![Rename Project](./pictures/mcx-project-rename.png) ## Variables Reference Variable substitution is supported in mcuxpresso-tools.json for defining paths (like: toolchainPath, sdk.path). You can use environment variables, like: `"toolchainPath": "%HOMEPATH%/.mcuxpressotools/arm-gnu-toolchain-12.2.rel1-mingw-w64-i686-arm-none-eabi"`. The following predefined variables are supported: - `${userHome}` - the path of the user's home folder - `${workspaceFolder}` - the path of the current project - `${workspaceFolderBasename}` - the name of the current project - `${pathSeparator}` - the path separator used by the operating system