Getting Started with Matter examples on NXP MCU platforms (MCUX SDK/FreeRTOS)#
This guide provides step-by-step instructions to build, flash, and test Matter examples on NXP MCU platforms.
Important: This guide covers Matter development for FreeRTOS-based platforms using MCUX SDK only.
For Zephyr-based Matter development, refer to the Matter Zephyr documentation.
VS Code Integration: The build, flash, and debug described in this guide can also be performed through the MCUXpresso for VS Code Extension, which provides a graphical interface with automated setup.
Prerequisites#
Before proceeding, make sure that all required software tools are installed and the MCUX SDK with the Matter environment is properly set up. Follow the installation guide for detailed instructions.
You also need an NXP MCU board that supports Matter. Refer to the supported platforms for the complete list.
Build Matter example#
List the project information#
Use the west list_project command to view supported boards and their available configurations. The command can be used following this structure :
west list_project -p examples/matter_examples/<example_name>/mcux
You can further filter the output by board or use a glob pattern to list all Matter examples supported by a specific board.
For instance, the following command lists all the Matter examples and configurations supported by the FRDM-RW612 board :
west list_project -p examples/matter_examples/**/mcux -b frdmrw612
Build the project#
Before building a Matter example, make sure that the Matter virtual environment is activated. You can do this using the activate script as shown below. If you’ve already run the bootstrap script in the same terminal session, you can skip this step.
For Unix-type systems (Linux/MacOS):
user@ubuntu:~/sdk-next/mcuxsdk$ source middleware/matter/third_party/nxp/nxp_matter_support/scripts/activate.sh
For Windows systems :
C:\sdk-next\mcuxsdk> .\middleware\matter\third_party\nxp\nxp_matter_support\scripts\activate.bat
Next, export the ARMGCC toolchain path using the environment variable ARMGCC_DIR. For example :
export ARMGCC_DIR=/home/Desktop/.matter_tools/arm-gnu-toolchain-14.2.Rel1-x86_64-arm-none-eabi/
To build Matter examples, use the west build command with the following syntax :
west build -d <build_dir> -b <board> examples/matter_examples/<example_name>/mcux
Additional arguments that can be passed to the west build command line :
--config release: This parameter can be added to build in release mode. The default build type isdebug.-DCONF_FILE: This variable can be used to provide a custom project configuration file. When used, the specified configuration files are merged as the application configuration. The variable must be provided with an absolute path of the custom prj.conf.-Dcore_id: If the board is multicore, this parameter can be used to specify the core ID targeted for the build.
Note about debug configuration: While the default build type is
debug, it only enables debug options for the SDK and application layers. To enable debug symbols for the Matter (chip) module libraries as well, add-DCONFIG_DEBUG=yto your build command.
For instance, the following command builds a Matter Thermostat example with Matter-over-WiFi and OTA enabled for the RW612 platform :
west build -d build_matter -b frdmrw612 examples/matter_examples/thermostat/mcux -DCONF_FILE=middleware/matter/examples/platform/nxp/config/prj_wifi_ota.conf
To configure your build further, you can either edit the Matter
application prj.conf, or provide your custom prj.conf in the build command
line using the -DCONF_FILE.
To use multiple custom prj.conf files, separate them with semicolons as shown below :
west build -d <build_directory> -b <board> examples/matter_examples/<example_name>/mcux -DCONF_FILE="/path/to/prj_<custom1>.conf;/path/to/prj_<custom2>.conf;/path/to/prj_<custom3>.conf"
You can also set Kconfig symbols directly in the build command using
-DCONFIG_<symbol>=<value>. For example, adding to the build command line
-DCONFIG_CHIP_DEVICE_DISCRIMINATOR=0xF01 sets the discriminator Kconfig
CONFIG_CHIP_DEVICE_DISCRIMINATOR to 0xF01 (3841 in decimal).
You can also modify the configuration using the Kconfig GUI. However, these changes are temporary and are lost after wiping the build directory. For more information about how to configure the project with Kconfig GUI, you can refer to the config project section in the MCUX documentation.
Flashing Matter example#
To flash a Matter example to your board, use the west flash command. For example:
west flash -d build_matter -r jlink
Use west flash -h to view all supported arguments, and west flash --context for runner-specific options.
To enable the west flash support in your environment, refer to the Flash and Debug The Example.
Platform-specific requirements#
NBU image (for MCXW72 platforms)#
For MCXW72 platforms, you must flash the NBU image before flashing the Matter application. Normally the NBU image should be written/updated only when migrating to a new NXP SDK or to a new Matter release.
Prerequisites:
Steps:
Locate the NBU image in your Matter source code tree:
mcuxsdk/middleware/wireless/ieee-802.15.4/bin/mcxw72/mcxw72_nbu_ble_full_15_4_dyn.bin
Use the blhost tool from the NXP LinkServer for Microcontrollers to write the image on the board:
blhost -p <assigned_port> write-memory 0x48800000 mcxw72_nbu_ble_full_15_4_dyn.bin
Additional binaries for OTA and Factory Data#
When building Matter examples with specific features enabled, additional binaries may need to be flashed before flashing the main application:
MCUboot bootloader (when OTA is enabled - RT1060 and RW61x platforms)#
If you built your Matter example with OTA support enabled (for example, using prj_wifi_ota.conf) on RT1060 or RW61x platforms, you must flash the MCUboot bootloader binary before flashing the main application. The MCUboot binary can be found in your build directory at:
<build_dir>/modules/chip/mcuboot/mcuboot_opensource.elf
Flash the MCUboot bootloader first, you can use JLink:
loadfile <build_dir>/modules/chip/mcuboot/mcuboot_opensource.elf
Note for MCXW platforms: For OTA functionality on MCXW72 platforms, refer to the dedicated Matter OTA guide on MCXW7x for platform-specific instructions.
For detailed information about OTA functionality and MCUBoot on supported platforms, refer to the Matter OTA guide on NXP RW/RT.
Factory Data (when factory data is enabled)#
If factory data is enabled in your build configuration, you need to flash the factory data binary. You can automatically generate your factory data during build by adding the extra argument -DCONFIG_CHIP_FACTORY_DATA_BUILD=y to your west build command.
The factory data binary can be found at:
<build_dir>/factory_data/factory_data.bin
For detailed information about factory data provisioning, refer to the NXP FreeRTOS platforms documentation.
Important note for MCUXpresso for VS Code Extension users#
When using the MCUXpresso for VS Code Extension, the extension’s flash buttons only handle flashing the main application binary. If your project uses additional features or specific platforms, you must manually flash the required binaries as shown above before using the extension’s flash functionality. This is required for the application to boot properly and for debugging to work correctly within the VS Code environment.
The typical flashing sequence when using a VS Code extension with OTA enabled is:
For MCXW72 platform:
Manually flash NBU image (required for all MCXW72 applications)
Manually flash factory data (if factory data enabled)
Use the VS Code extension flash button for the main application
For RT1060/RW61x platforms:
Manually flash MCUboot bootloader (if OTA enabled)
Manually flash factory data (if factory data enabled)
Use the VS Code extension flash button for the main application
Testing Matter example#
To test Matter examples on NXP MCU platforms, we recommend following the guide provided in the connectedhomeip repository : Testing the example.